FAQ: What is readback time for current measurements on the 6600 series power supplies?

Internal current measurement take about 100 milliseconds to be performed. If measurements are performed over the GPIB, an additional 50 milliseconds is required for communications.

Applies to: 6641A, 6642A, 6643A, 6644A, 6645A, 6651A, 6652A, 6653A, 6654A, 6655A, 6671A, 6672A, 6673A, 6674A, 6675A, 6680A, 6681A, 6682A, 6683A, 6684A, 6690A, 6691A, 6692A

Select Home to return to the table of contents for more FAQs.

Visit our Power Products Forum for additional topics and discussions.

Read technical postings on our Power Blog – Watt’s Up?